Other Parts Discussed in Thread: LMH5401,
Hi,
Would it be possible to share the measured s-parameter data for the LMH3401 and LMH5401?
Thanks,
Apurva Gowda
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Apurva,
I have attached the measured S-parameter data for the LMH3401 and LMH5401 with differential input and output configuration (4-port). I would recommend you to start analyzing with the files only for frequencies >70MHz as the VNA dynamic range is very bad at lower frequencies less than 70MHz.
Also, do you need the measured S-parameter data for the single-ended input to differential output as well?
Best Regards,
Rohit
Thanks Rohit! Yes, we would like measured S-parameter data for the single-ended input to differential output as well.