Other Parts Discussed in Thread: THS4631, TINA-TI
I have a few questions regarding TIA noise analysis (specifically for OPA657):
1. SNOA942A, Table 1-> All noise terms are shown in units of pA/RtHz. My understanding is that this is because the noise was modeled as an input current source. Since I need to establish a noise floor on the output in Volts, do I multiply a noise term with the feedback resistor gain Rf to obtain the output noise.
For example, in Table 1, for the THS4631, the noise voltage term is 8.7 pA/RtHz and Rf = 810 Ohms. Is the output voltage noise 7047pV/RtHz (=8.7pA/RtHz * 810 Ohms)?
2. SBOA060 -> I follow the voltage noise calculation, but I do not follow the current noise and resistor noise calculations. Can someone elaborate on those calculations?
3. Are there guides on SPICE simulation for TIA noise?