Dear Team:

 Our customer used TLV2401 Pspice model to do voltage follow circuit simulation, but the output current over datasheet spec.

Customer also done other amp. pspice model by TIna, but the output current stil high over datasheet spec.

Could you check it for us?

As below is customer question description:

Per described, we also test Ti-Tina on TLV2401, TLV2402, OPA704 parts.  The result as the same below, the OP output current can source the high current over than spec, and in the voltage follower circuit the output voltage still set in fix voltage, no drop. That’s quite different with real test result that will drop the output voltage even down to only few hundred milli-volt from 3.3V.

 

Can you help to find out the over current situation on these OP library?