In OPA333/2333 datasheet open loop voltage gain (Aol) is 130dB typ, Rl= 10Kohms, found in electrical characteristics.
However, the curve for Aol x freq. shows something quite different, even at lower freq. (10Hz).
What am I missing??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thiago,
What you are missing in your consideration is the fact that the open-loop gain (AOL) decreases with frequency at -20dB/decade and since 20*log(1)=0 at the unity-gain frequency, AOL=0dB at f=350kHz.
Therefore, AOL PDS spec of 130dB (3,160,000) refers to DC AOL and to find out where AOL will flatten out to -3dB DC value you need to make following calculations: DC_AOL = Unity-Gain_Bandwidth/DC_AOL = 350kHz/3,160,000=~0.1Hz
Thus to see DC AOL, you need to look at AOL curve below 0.1Hz - see AOL simulation below.
The OPA227 specs an AVOL = 160dB and have a full curve: 0.01Hz to 10MHz,
I suspect the difficulties are with the measurement equipment. Depending on the test circuit, I imagine the error voltage being measured could not be distinguished from the system noise.
Regardless it would be nice to see consistency with the datasheets. Perhaps real world measurements backed up with silicon simulations at the transistor level to provide a full curve rather than leaving it up to the customer to calculate an expected response.
-Ken