Good morning
I use a OP OPA2277UA in the configuration load cell shown in Figure 3 of the datasheet. since the two OPs in the same houses, the drift is compensated?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Good morning
I use a OP OPA2277UA in the configuration load cell shown in Figure 3 of the datasheet. since the two OPs in the same houses, the drift is compensated?
Thanks
Fabio,
Both channels of OPA2277 dual op amp are laser trimmed virtually to zero but the physical stress associated with the packaging of the die causes the random shift in the input offset voltage and drift. For that reason, there is no correlation between the two channels of the dual op amp in Vos drift - one channel may have a positive drift while second channel of the same package may have a negative drift. In short, the probability of the same Vos drifts in both channels of a dual op amp is identical to the probability of two single op amps having the same drift.