We want to build an circuit of water cutoff
Controlling of water pump motor that adding\stop adding water to a container
The water container maid of metal and the signal in the water should be AC Signal (square 5V)
The body of the container connect to GND
I have only one Entrance\inlet to the container so with the AC signal
I should also fit the AC Signal to the water and also sense the present's of the water
(We must use AC signal)
Another issue - I need design sensitivity of water that my probe feel's (sense) 20Kohm\50Kohm\100Kohm
with AC signal that fitting probe sense
I thought of some idea's
like Voltage divider with the water resistance
or current flow measurement - when my fitting probe (AC Signal) close circuit with the water to container body (GND)
Of course we are using MCU with ADC to measure analog signals
Please suggest more ideas how can I over come that problem
Measure the present's of the water and sensitivity to water resistance
Thanks in advance
Mayer