Although the customer is estimating TLV2374, breakage takes place and it is checking the cause.
The cause considered to be a circuit diagram was written to attachment.
If there is a cause otherwise considered, please let me know.
[Supplementary information]
・A power supply uses a stabilized power supply.
It wired by a 1m cable, and circuits of TLV2374(s) have connected by 40cm wiring again,
after passing along the capacitor bank of 2200uF.
・Although the power supply is usually stable, if the temperature controller for an examination is used,
the random noise of about a maximum of 200 mVP-P will occur.
⇒The same noise comes out with amplitude also with a comparable output (1pin and 7pins) of TLV2374.
Is an oscillation excited by this random noise and is a device damaged?
Thank you for your consideration.