I'm looking at using an IVC102 amplifier for integrating a current from a PMT. The expected range is within 1 nA - 5 µA and the requested integration times are in the second range. To not saturate the sensor (if I've understood things correctly) I would need to use a large external capacitor to do this (µF).
Would this be expected to work, considering that my capacitor would be several orders of magnitude larger than the internal ones?
Many thanks and best regards
Mikael