Hello,
I plan to use an INA826 at unity gain, with small (<20 Ohm) series resistors on its inputs (this resistor value cannot be increased for a number of reasons). It is critical to know at least one of the following overload parameters:
1. The maximum input current (at inverting or non-inverting input) of the INA826 at 25oC, when a +/-15V input overvoltage occurs and the device is powered off. That is, when both supply pins are at 0V.
2. The same parameter at +85oC.
The problem with the datasheet (figure 17) page is that it provides only typical values at non-zero supply voltage and room temperature. I could extrapolate the temperature coefficient of the threshold voltage of the internal FET limiter. I could also made some assumptions for the power-off condition. But the spread of the threshold voltage (from part to part) is still unknown and quite unpredictable. At least I could make some fair assumptions if I knew that spread (say, within 98% confidence value).
Thank you in advance