Hi
I am using LMP91200 evluation board and SPIO-4 board for sensor test. In SPIO-4 board contain Spratan-6 XC6SLX16 (FPGA) and Atmel SAM3U microcontroller. These board connect to each other by GPSI 32 pin connector and it connect to my laptop by USB cable. Output of ADC is connected with FPGA. Output of sensor got in sensor AFE software.
I have a dought doubt , When we do the sensor testing which works either microcontroller or FPGA and both.
I am desinging pH meter. If both or single processor will work then FPGA is required for pH meter.