Hi,
I use the LMP7721 to build a charge amplifier. Two 560K resistors are used to divide the 3V single supply. So I get the 1.5V as the commen mode voltage and have it connected to pin 'V+'. Feedback Rf of 1G ohm and Cf of 10 pF are connected in parallel between pin 'V-' and pin 'Vout'. Pin 2 and Pin 7 are used to build the Guard. Guard trace is connected to pin 'V+'. The charge amplifier design refers to Figure 6 of OPA129 Datasheet.
The problem I encountered was the potential of pin 'V-' is 0.9V, not equivalent to that of pin 'V+' 1.5V. This may cause LMP7721 saturated, and thus we can't get the right signal output.
Happy to hear your advice.
Thanks,
Eric