Hi Ti people,
I would like to know if there is a specific failure mode of the LT1013 precision amplifier when applying a voltage over the absolute maximum ratings defined in the datasheet of this component.
For example, if I use the LT1013 as a comparator, which will be the output state (+Vsat ?, -Vsat ?) when
- supply voltage Vcc+ exceeds 22V
- supply voltage Vcc- exceeds -22V
- differential input voltage exceeds +/-30V
Thx,