Hi all,
Samsung inquired for the circuit of pulse generation using TLV3501 and OPA357.
The circuit is as below.
They did simulation using Tina file for triangle wave generator that you gave me at E2E before. However, they could find that the triangle wave is changed depending on the value of resistors. Even if the value of resistors was changed a little bit, the triangle wave was changed much.
So the question is how much tolerance of resistors has an inpact on the period(or frequency) of total PWM pulses when the PWM pulses are generated through comparators after triangle wave occur.
That is, they would like to know the range of error due to the resistor.
The reason why they asked this question is that there is +/- allowable tolerance frequency at specific frequency range.
Also, when the capacitances are added at Vref, how much the capacitances have an influence on output voltage. (that is, parallel capacitor at Vref for both of TLV3501 and OPA357)
Would you give me the answers as soon as possible?
Thank you.
Warm regards,
Sammy Jeon.