Circuit simulation and why not, high input impedance input charge signal output, why not ah, DC bias is wrong
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Circuit simulation and why not, high input impedance input charge signal output, why not ah, DC bias is wrong
Hi Shuai,
Yes, it appears that your dc bias arrangement is not correct. The 2N7002 and 2SA4127 transistors shouldn't turn on and the 4 mA from the current source must be forced through the series 30 k and 200 k resistors. That would result in a very high voltage being developed across them. The output voltmeter is indicating 0 V, but that may just be a default if the circuit isn't correct.
The reason I say the transistors shouldn't be "on" is because of the bias conditions of the 2N7002. The 2N7002 gate threshold voltage is on the order of +1 to +4 V. If the input generator impedance is low, the 200 Ohm resistor connected to the gate provides a low resistance path to the MOSFET's source. The 100 Meg resistor, connected from the 200 Ohm resistor back to the 200 k/30 k resistor divider also acts as a very large voltage divider. The voltage on the gate ends up being microvolts which is completely insufficient to turn on the MOSFET. If the MOSFET is off, there isn't any current flow through the 1.5 k resistor would be needed to bias the PNP base-emitter junction. Therefore, the PNP should remain off too.
The ac input generator would have to develop a positive dc large enough to overcome the MOSFET threshold voltage for the MOSFET to turn on. When the ac input level falls below the threshold voltage the MOSFET would turn back off.
Regards, Thomas
PA - Linear Applications Engineering
Hi Thomas
This is my ICP circuit, two wire, a ground wire, a is the output and power line, power 4-20mA, 28-30V power supply, circuit practice I no problem, is my simulation circuit is wrong, do not know where the problem,It is a constant current source is wrong
Hi Shuai,
I would also recommend that you look into some integrated 4-20mA transmitter circuits from Texas Instruments. You can view through our portfolio here:
http://www.ti.com/lsds/ti/amplifiers-linear/4-20mA-conditioning-products.page?paramCriteria=no
Hello
I mean, you may not know, constant current source 4-20mA I, 28V-30V power supply, not the output mode
Hello Shuai,
I am unable to understand what your circuit applications is. Can you provide a brief explanation?
Regards, Thomas
PA - Linear Applicaitons Engineering
Hi Shuai,
As we suggested in the post: http://e2e.ti.com/support/amplifiers/precision_amplifiers/f/14/p/339856/1192345.aspx#1192345
You will need to use a charge-amplifier to acquire the signal from your charge-based sensor. Then you will need to derive a DC output voltage based on the sensor output. This can be accomplished using an absolute value circuit after the charge-amplifier output. Once you have a circuit that produces a DC output voltage proportional to your sensor output you can connect that voltage to the input of one of our XTR devices, such as the XTR117.
I've attached a presentation that discusses charge-amplifiers and includes circuits to convert a capacitive sensor to a DC output. You will need to design and test the circuit on your own based on the performance and functionality you desire.