I would like to confirm XTR111 operation.
The customer uses XTR111 without regurator operation. In this case, the problem occured.
In the case of OD="High", VG voltage was higher than IS votage + 7V. (I think IS voltage is higher than VG voltage.)
For this problem, I have questions.
1. Is this correct operation?
2. How much is minimum IS volage (How much does IS voltage turn down)?
3. In the datasheet, IS voltage should be higher than VSP - 6.5V.
But in this case, IS voltage was lower than VSP - 7V.
Do they need to add the circuit for keeping IS voltage?
Or are there any problem in their circuit?
The circuit is;
- without current limit circuit (bipolar transister)
- They does not use the regurator
- REGF connects REGS through the resistor (10kohm)
- VSP = 12V
- VIN = 5V
Best regards,
Atsushi Yamauchi