Hi All,
Please let me ask about Input Overvoltage (IOVerr).
- Please confirm the threshold of IOVerr. I can't find it in datasheet.
- Is this function just only set flag or protect (clamp) in addition?
Best Regards,
Sonoki / Japan Disty
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All,
Please let me ask about Input Overvoltage (IOVerr).
Best Regards,
Sonoki / Japan Disty
Hello Sonoki-san,
To prevent triggering IOVerr, ensure that the input voltage remains between (VSN + 2.5V) and (VSP - 2.5V). IOVerr is not a clamp, only an error flag. However, the PGA280 input pins do have internal diodes connected to VSP and VSN which activate when the input signal exceeds VSP or VSN.
Best regards,
Ian Williams
Linear Applications Engineer
Precision Analog - Op Amps