I have a question about the REF pin. My impression is that if my signal is AC and I want to use a single supply, say 5V, I should put 2.5 volts DC on the ref pin. If this is correct, is it possible to put a TLE2426 with a BUF634 on the ref pin to supply the offset ? Also, does this imply that if a have an input signal which is pure AC, the zero of the output will be at 2.5V ?