Hi
can you provide me Tj data of LM339APWR and TL431ACDBZR?
I try to calculate by Tj = Theta Ja * Pd + Ta
but for those part, i do not know how to get Pd.
So please let me know how to get Tj data.
thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Kevin,
Pd the TL431 is VKA * IKA
VKA and IKA are set by application.
Pd for LM339 is sum of VCC * ICC and IOL * VOL for each low output.
VCC and IOL is set by application.
ICC and VOL values can be found in data sheet.
Hi Ron,
I calculate it, and can you help me to double confirm that?
thanks.
Pd the TL431 is VKA * IKA
VKA and IKA are set by application.
Check datasheet Recommended operation condition
Vka=36v
Ika=100mA
TL431ACDBZR Theta JA=206 C/W
1. 36x100=3.6w
2. 206x3.6=741
3. 70+741=Ta
So Ta=811? is it correct?
Pd for LM339 is sum of VCC * ICC and IOL * VOL for each low output.
VCC and IOL is set by application.
ICC and VOL values can be found in data sheet.
VCC=5V
ICC=2mA
5X2=0.01W
IOL=16mA
VOL=400mV
16X400=0.0064w
0.01+0.0064=0.0164w
LM339APWRTheta JA=113 C/W
Tj= 25+113x0.0164=26.85
Kevin,
Pd the TL431 is VKA * IKA
VKA and IKA are set by application.
Check datasheet Recommended operation condition
Vka=36v Ika=100mA
While 36V and 100mA is allowed. It is not practical to do both at same time.
For example, application has VKA = 5V and IKA = 10mA.
TL431ACDBZR Theta JA=206 C/W
1. 5V x 10mA= 50mW
2. 206C/W x 50mW =10.3C
3. Ta + 10.3C = Tj
Pd for LM339 is sum of VCC * ICC and IOL * VOL for each low output.
VCC and IOL is set by application.
ICC and VOL values can be found in data sheet.
VCC=5V; ICC[max]=2mA
P = 5V X 2mA =0.01W
IOL=4 * 4mA; VOL=400mV
P = 16mA X400mV =0.0064w
0.01+0.0064=0.0164w
LM339APWRTheta JA=113 C/W
Tj= 25+113x0.0164=26.85
Correct