Hi,
I need to read 6 x 4-20mA sensors. My current design utilize Instrumentation Amplifier TI INA332 and RC filter to eliminate the digital HART signal that is coming from the sensors and TI ADS1115 16 bit delta-sigma ADC. As shown in the following diagram.
I've got concerned when Ed Mullins mentioned in TechDay that the InAmp should be powered with the same voltage of Vbus. Could anyone please elaborate if this would be a problem for my circuit. Because to my understanding the voltage across RCS13 will not exceed 0.5V and after amplification it will be less that 2.5V.
I would like to hear opinion about using Current Shunt Monitors like INA3221 (triple channel I2C CSM) to perform the task. Especially in regard to the filtering of the digital signal. Or any other design that would be lower in cost or more reliable.
Thanks,
Edd
EDIT: the image was re-uploaded