I have a board with a PGA280. The Analog supply is connected to +/-12V, VSop = 5V, DVdd = 3.3V.
I'm currently using the power on Reset values for all the settings (1/8V, 1:1, etc).
InN1 is connected to GND
InP1 is connected to a signal source (100hz, -5V to 5V sinewave)
Vocm = 2.048V
What I don't understand is why the outputs: Vop = (100hz sinewave from 2.1v to 2.775V) and Von = (inverted sineware from 2v to 1.32V).
Shouldn't these signals be centered around Vocm (or 2.048V)? and the sinewave crossing over the Vocm level?
What am I missing here?
thanks in advance for your help
Matthew