Hello,
I want to generate a square wave current signal in the frequency range of 1Hz to 20KHz of peak amplitude 20mA. So i was thinking of using a XTR111 V to I converter with output current set to 20mA and then switching its output on and off using a MOSFET as a switch, which will simply connect load to XTR111 when on and disconnect it when off. This MOSFET will be driven by a Frequency generator generating the gate signal for MOSFET in the frequency range from 1Hz to 20KHz. Will XTR111 have any issues in switching its output current at 20KHz or lower ?