Hi,
I use the 10-bit DAC DAC5652 to generate a trapezoid waveform,
the rising time and the falling time are 2us, the hold time is almost 2us.
The following is the waveform I measured from the input pin(PIN 2 +) of TLE2142.
Q1 But I found a gap at the rising edge, it is almost 1V in this case as following,
what is this? and how can I tackle this?
Q2 The slew-rate of TLE2142 + Buffer is extremely slow,
in the spec the min slew-rate of TLE2142 is 27-V/us and the buffer is 75V/us. How can I improve it.?
The following is the sch of power amp, but I only keep the buffer stage of the power amp.
The probe point of above figure is TP68, There is no load on the point.
The TLE2142 is powered by +36 and 0V