Halo everyone,
I already tried AMC1100 on AC sensing, and it give good sine wave.
Now, I am curious whether I can use AMC1100 in DC voltage sensing,
if can, do I have to scale the sensing range to 125mV.
Since AC sensing range is 250mV.
And I have other question in mind.
The function of R1 and R2 is to supply 2.5V to VNN? Is this really needed?
And can I know the function of C3, if I want to sense DC voltage, do I still need the C3?
Sincerely
Tan Chin Yew