Hi, I am trying to evaluate PGA309EVM-USB eval module refering the user guide http://www.ti.com/lit/pdf/sbou084 . The SW used is downloaded from http://www.ti.com/lit/zip/sboc320. I have 11 pressure points ( bridge output) for 17 temperatures and would want to emulate the sensor for all these pressure points. However, emulating the sensor (using the jumper settings, not with the external sensor) i.e DAC voltage generation ( wrt 11 pressure points for 17 temperatures) using GUI is not so clear. User guide page number 49 ( of sbou084) says 'Enter raw bridge sensor data', there i am seeing the options to enter the offset i.e bridge voltage for 0psi and full scale ( for the maximum psi) in step 3. As per my understanding, it is for span and offset correction over the temperatures to have an accuracy less than 0.1%. In step 4, there is option to enter data for 0psi, full scale and midscale psi. This is for nonlinearity correction. I'm not finding any option to simulate the sensor for 11 pressure output over temperatures using GUI. Also, i didnt understand page number 33, what is this for ?? I refered the obsolete version PGA309DK, how to emulate the sensor using the potentiometers and switches was explained in detail in it's user guide. Kindly clarify these points at the earliest.
Thank you so much.
Regards,
Leni