Hello.
The customer wants to use it as VI converter of the output (0-40mA) for input (0-10V).
And the customer is going to use XTR110.
Expand SPAN by connecting resistance between 1 -16 pin pins in parallel with internal resistance R9 (datasheet Figure 1.), and do not have any problem?
It means whether there is possibility of destruction and the trouble in a customer wanting to know it.
The customer thinks that the problem of precision, the error is restrictive.
Actually, using internal R9 (50 Ω), connect external resistance (51 Ω) more between 16pin and 1pin, and do it to 25 Ω by composition resistance, and be that I double a span and use it.
Regards.
K-hashi.