Hi,
I would like to detect threhold current of 2.5uA, so i require a current shunt that has low input current. Is there any current shunt with voltage out put i can use? Also, due to mechanical constrain, my package cannot be more than 1mm height.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I would like to detect threhold current of 2.5uA, so i require a current shunt that has low input current. Is there any current shunt with voltage out put i can use? Also, due to mechanical constrain, my package cannot be more than 1mm height.
Hi, I prefer high side sensing in my design. LT6118 seem like meet the requirement, due to low input offset current. Pls advise is there solution in TI to meet 2.5uA threshold current in Avalanche photo diode.
Hi Kwan,
Please share with us the system details like supply, bus voltage and a schematic if possible. Also are you trying to implement something like this TI design http://www.ti.com/lit/ug/tidu535/tidu535.pdf. I am moving this post to Precision Amplifier forum and someone will assist you soon.
Hi Rabab,
It’s high side sensing.
The common mode voltage is 3.3V typ.
The design is quite simple. There is a current source which provides 0mA(min) to 2mA. This is connected to ADC in our controller IC. Beside this, I want to sense 5uA and 10uA to alert the low current.
When it is 5uA, the alert should be on. When it increased to 10uA, the alert should be off. In order to avoid the fluctuation of the alert, I need about 5uA hysteresis.