Hello, i´m using a LMP8601 amplifier to convert a 4-20mA current loop into a voltage signal to bring it to a ADC, i´ve mounted the circuit as it shown in the datasheet and used a 0.01 Ohms resistor as Rsense, but the IC is not responding when i plug the 4-20mA terminals of a Fluke into the IC pins. Does anyone have idea why is not responding?
Thanks in advance.