We are developing a product with a 380Vdc high resistance mid-point ground power distribution system. I need a cheap and simple ground fault detection circuit and attached below is what I have come up with so far. I need to isolate the high voltage DC from the control circuitry. A micro-controller will monitor the output of the ADS1013 ADC to detect a ground fault. If there are no shorts from the +/-190Vdc rails to chassis gnd, the output of the OPA244 will be 0V and the differential output of the AMC1200 will be 0V. If the -190V rail shorts to chassis gnd, the OPA244 will go to ~0.25V and the diff output will go to ~2V.
This doesn't have to be ultra precision, I just need a way to detect if one of the high voltage rails have shorted to chassis. I want the digital output so that I can set the "trip" point in software depending on how sensitive we need the detection to be. So the question is: are there better parts that I could use to accomplish this function?
Thanks