We have tested the given circuit using INA125P DIP package. At the 16th pin , we got 10V with respect to ground , to power up the load cell. Also we have given the output of the loadcell to pins 6 and 7 of INA125P with a gain resistor of 220ohms and we received the output (at pin 10 ) correctly. But now we are using INA125UA SOIC package instead of the INA125P .With same circuit given below, INA125UA is giving only 0.22V at 16th pin instead of 10V. So we are not being able to power up the loadcell using INA125UA. Why we are not being able to get 10v at 16th pin of INA125UA using the same circuit. Kindly help us as soon as possible.