Hello,
I would like to teach me about behaivor of out of LM13700's operating range.
LM13700's operating range is until 0 degree.
However, the customer had test of LM13700 that changes temperature until -20 degree.
And LM13700 could output until -18 degree.
So the customer would like to use LM13700 until it with understanding out of specification.
(It means they don't need us product warranty.)
If LM13700 is used until its degree, they have concern for infuluence to correct behaivor.
Does LM13700 have cause to stop or move with strange when LM13700 has behaivor in negative degree?
(For example, LM13700 stops in ratch up, and so on.)
Best regards,
Mitsuo Hirata