HELLO THIS IS HOT
I NEED TO NO IF THE PIN OUT IN THE DRAWING IS CORRECT
WHAT I NEED TO NO IS THAT IF I HAVE A SINE WAVE FEF. ON THE X (+) INPUT AND THE NEG. INPUT TO GROUND .
VOUT OF THE PART IS TIED TO Z1 AND Z2 WILL BE MY SUMMING NODE FOR CURRENT SENSE SIGNAL.
NOW I HAVE FROM THE OUTPUT OF THE INVERTER A SENSE NETWORK AND A POT THAT I WILL USE TO ADJ. THE OUTPUT VOLTAGE THIS VOLTAGE WILL GO INTO THE Y(-) INPUT AND THE (+) IS GOING TO GROUND .
NOW WHAT I NEED TO HAPPEN IS
AS THE FEEDBACK SIGNAL ON THE Y(-) INPUT BECOMES GREATER THAN THE SINE REF THE OUTPUT SINEWAVE WILL START TO DECREASE
AND AS I ADJ ARE TURN R3 ON THE DRAWING I CAN MOVE THE SET OUTPUT VOLTAGE UP AND DOWN AND ONCE I HAVE THE OUTPUT CORRECT I START TO LOAD THE OUTPUT OF THE INVERTER AND YOU SHOULD SEE THE OUTPUT FROM THE MPY634 INCREASES TO TRY AND MATCH THE SIGNAL OF THE FEEDBACK TO IT MAINTANS REGULATION
LET ME NO ARE UPDATE THE DRAWING AND SEND IT BACK TO ME AND I WILL MAKE THE CHANGES HERE.................
SO THE MAIN IDEA HERE IS THE REF SIGNAL ON THE X INPUT IS CONSTANT IN AMPLTD. SO I NEED TOHAVE THE SAME AT THE OUTPUT OF THE MPY634 AND WHEN I APPLY A FEEDBACK SIGNAL THE V OUT SIGNAL SHOULD DECREASE AS MY FEED BACK SENSE SIGNAL BECOMES GREATER THAN THE REF SIGNAL
GET BACK PLEASE ASAP
THIS IS HOT