Hi, good evening. I'm measuring an AC current of 50mA @ 5A and must be less than 50 ms its response. This, I've got a TC and an array of opamp peak detector and a filter at the output to try to make it as similar to a DC signal, but I have some questions. If I want to measure the amplitude, this configuration is valid for OPAMP (peak detector)? I say this because I am not measuring the negative part of the AC signal and do not know if losing accuracy and speed of detecting a change in current.
Cheers
LAMC