Hi all
Would you mind if we confirm about TL022C?
<Confirmation>
Absolute maximum ratings are Vcc+ : +18V, Vcc- : -18V, in case of using single power supply, it will be 0V - 36V.
When the single power supply is 0V - 36V, Absolute maximum ratings of input voltage is 0V - 30V, isn't it?
And then, recommended input voltage will be 0V - 26V, won't it?
Kind regards,
Hirotaka Matsumoto