I am using evaluation board for LMP7721 with single 5V supply in inverting transimpedence amplifier with offset. In this case the non-inverting terminal and gaurd would be at 2.5 V. This amplifier would be for ionization chamber with output with respect to ground (no gaurd connection). My doubt is whether to use
1) A BNC connection at input of evaluation board or
2) A traixal connection at the input of evaluation board and leave gaurd connection open at the ionization chamber.
or there is any other method to do the connections.