Hello,
In the customer evaluation, they measured gain peaking at 200kHz.
Is this device has peaking at 200kHz?
Conditions are the fllowing.
Application : Voltage folower
V+ =15V
V- = 15V
RL=2kohm
CL=100pF and 1000pF, ( the peak is increased with large capacitive drive)
RF=100kohm (connect between output and negative input)
CIn=1uF (connect between negative input and GND)
I can send the customer measurement wave and schematics if you contact to the following e-mail address.
asaka-r@clv.macnica.co,jp
Best Regards,
Ryuji Asaka