can anybody help me , if INA122 can be used for calculating glucose levels using the IR LED receiver and transmitter sensor. can INA122 or suggest the right Amplifier to detect Glucose using SFH7050.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Jagannathan,
I am moving your post to the Precision Amplifiers forum that covers this device.
Dear Mr. Pete Semig,
Greetings for a Great New Year. Two help I need from you,
1. SFH 7050 has a peak wavelength of 940 NM, Can you help us to understand if we can detect Glucose using this IC.
2. AFE4490 has a built in Transimpedence amplifier. Do u think this can be used instead of TIPD176. or do u suggest we must use TIPD176.