Hi all,
I'm using a LM331 as a voltage to frequency converter and I observed a weird oscillation on PIN2.
I put the LM331 on a solderless board using the component values shown in the datasheet (http://www.ti.com/lit/ds/symlink/lm331.pdfand adding power supply decoupling capacitors of 100nF-1uF.
I grounded the input in order to avoid comparator triggering. The datasheet shows a typical current range from PIN2 of 10uA to 500uA, so if a 1.9 V reference is used, then Rs maximum value should be 190Kohm.
I put the circuit inside a grounded/shielded aluminium case to avoid EMI.
In this condition if I use a Rs value higher than 10Kohm, then oscillation appears on PIN2. This oscillation is at 65-100Khz, and seems pretty regular once Rs value is fixed. The amplitude is around 100-200mV.
If I let Rs to float, then the terminal connected to PIN2 oscillates, while the other is steady at 1.9V. (antenna?)
I'd like to know if this behaviour is normal or not (I suppose not).