Hello, Ian. I'm a Daekeon Woo from Autonics in Korea.
I have a problem when i calibrate on our products with Multi-Cal.
Now, i calibrate three temperatures(-10℃, 25℃, 80℃) with Master kit and Slave kit. But after calibrating, Many products don't save calibration data. They save only 80℃ data so the output at -10℃, 25℃ is an error. For example, The proper output is 1VDC at -10℃, 25℃ but the real value is 1.070VDC. It happens so frequently. I think it happens because it can't save proper calibration data. I want solve this problem.
When It occurs calibration fail on High Value during calibration, Can i click "Re Current Cal"? I often click this button when caibration fail.
I think when i click the button many times, It can't save calibration data to products.
I have other questions.
Now, I use Multi-Cal 2.1 version. I received this version last year. Is there its upgrade version? If you have a latest version, i want download it.
Also, i want to know the proper cable length using connectiong between Multi-Cal interface and our products. I think the shoter lengh is better than long cable length. Please let me know as soon as possible^^
Thank you for your cooperation.