Hi,
I am using ina 128 as a comperator in my project. I have used the basic connection that showed in datasheet in page 13. The gain resistor is 2k. I have applied the signal to Vin-(pin 2) input and the reference to the Vin+ (pin 3) input. I have noticed that when there is no signal in pin 2 and I have applied 4.2V to the pin 3, I get 940 mV in the other input (pin 2). Why this is happen? Is it normal? I am using this setup in very precision instrument so this make me fear about unexpected results.