This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question of LMV7271 for Hysteresis Circuit

Hola,

We used LMV7271 as our new design of hysteresis circuit as below:

Vin = 36V --> Vout : low

Vin = 39V --> Vout : high

And the calculated result as below:

But the actual result after we testing become as below:

Vin = 31V --> Vout : low

Vin = 40V --> Vout : high

Are there something wrong which about setting or missing? 

Another question is if I want to achieve this hysteresis function, does TI have another suitable solution or LMV7271 is the best solution?

Brs