Hi all
Would you mind if we ask OPA1688?
Our customer would like to make the following condition using OPA1688.
-Load : 128ohm
-Output power : 130mW
Above condition, following values are obtained;
-31.6mArms / 43.5mAp
-Vrms=4.11V, Vp=5.81V, Vpp=11.62V,
As the result, is it possible to use 128ohm with 130mW?
Kind regards,
Hirotaka Matsumoto