Datasheet of TL07 family mentions the output swing typical value to be +/- 13.5v but nothing has been specified for Maximum value of output swing, can anyone confirm that? Page 6 of datasheet
regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thanks Ron for the reply, could you please also confirm if i am correct to say that the differential voltage (mentioned in absolute maximum ratings section)
Absolute ((VIN+) - (VIN-)) should be maximum 30v ? regards Siddharth
HI
i tried to search in the datasheet of TL07 series but couldn't find Isc -
What is the output short circuit (Isc) current of TL07 series opamp?
regards
Siddharth,
Short circuit current come from the supply rail then there is a 1.5V head room (drop out) reduction, lastly there is a 200 ohm resistance to the output pin.
When output is trying to go high, Isc = (Vcc+ - 1.5V - Vout) / 200 ohms
When output is trying to go low, Isc = (Vcc- + 1.5V + Vout) / 200 ohms
Siddharth,
The 200 ohms output can be calculated by choosing two points on figure 6 and doing math.
It is also seen in figure 13, 64 + 128 = 192
Thanks for the reply, so can i safely assume that internal resistance between VCC+ to output is 200 ohm when output goes high and similarly from VCC- to output is 200 ohm when output tried to go low? regards
Siddharth,
Meet me halfway. What is your maximum VCC+ and VCC-? To what is the output shorted? (ground or some other node?)
thanks
VCC+ is 12v and VCC- is -12v
you can let me know for the worst case - like when the ouput load tends to 0 or output getting shorted to ground
please can anyone share the output voltage versus load current curve for TL07 series of OPAMP
Thanks Ron for all the help, i would also request you to please provide the curve for +/-15v case and single supply voltage case from 0-30v. It will be great help thanks
Hi Ron, request your feedback over the data for +/-15v and 0-30v, hopefully the Lab results hae arrived