I need an op amp with dual supplies 12V to -12V and has input overvoltage protection (30V to -30V) and also has protection against applying an input voltage before power up. Will OPA192 do it? If not, is there such a thing? Preferably SMD.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I need an op amp with dual supplies 12V to -12V and has input overvoltage protection (30V to -30V) and also has protection against applying an input voltage before power up. Will OPA192 do it? If not, is there such a thing? Preferably SMD.
Hi Tony,
If the user applies a voltage to your inputs before power-up, the internal ESD diodes will forward bias. If your power supply rails (when they are not powered up) have a path to ground through which the current can flow, then all you have to do is limit the current. If the power supply rails do not have a path for the current, then your power supply rails are floating, in which case it is harder to predict what path the current will take.
Regards,
Mihir