Hi all
Would you mind if we ask TL972?
The datasheet shows as follows;
-Output sink current : 80mA
-Output source current : 1.4mA
If the output voltage is -5V to 5V sin wave form like as audio, in case of -5V, the current will be sink current 80mA.
If case of +5V, we guess that this is source current 1.4mA.
So, they are the same value.
Our customer would like to use 80mA both case, so is it possible?
Kind regards,
Hirotaka Matsumoto