Hi,
I want to use the ALM2402A in a BTL configuration to drive a 32Ohm speaker, powered from a single 12V supply.
I used the TINA-TI simulation to test the circuit and I see that with 1K feedback resistors the circuit works fine and distortion is <0.5%.
If I increase the feedback resistors to lets say 20K the distortion increases to 5%.
Is the AML2402A not designed to handle higher value feedback resistors or am I dong something wrong here?
I tried to upload the schematic but do not see how I can do this. I can send the Tina schematic by email.