Hi,
I just purchased the OPA1S238xEVM evaluation module for amplifying my photodiode output. I am using a Thorlabs DET025A photodiode with the following characteristics:
Responsitivity: 0.35 (at my wavelength - 632nm)
Dark Current: 35pA (at 5V)
Diode Capacitance: 1.73pF (max)
Bias Voltage: 12V
Output Voltage: 0 to 2V
Max input power: 18mW
For my application, I do not expect the input power to be more than a few 10's of microwatts. I have no strict requirements for the voltage output of the circuit since I will be measuring with a DAQ of range -10 to +10V. The signal I will be measuring on the photodiode will have components up to 50MHz so the bandwidth of the circuit needs to match this.
Could someone please help with the optimum component values needed for this application? I see there are options to insert many components for changing the feedback and gain e.g. R1, C1, R5, R6, R10 etc. I tried using the WEBENCH designer for this, but it couldn't seem to match my requirements - unless I was doing something wrong?
Many thanks,
Jordan