Hi Team,
I have a customer that's looking to measure a 2V battery on top of a 40-80V common mode. The entire system is floating, so isolated signal delivery is necessary. Ideally, the battery can be measured down to 0V. We're looking at the ISO124 isolated amplifier, as well as isolated ADCs and non-isolated ADCs coupled with discrete digital isolators, but I was wondering if there was a recommended method to achieve this.
My thoughts:
- The isolated ADCs look promising, but they can't handle 2V differential, only 250mV.
- Discrete ADCs/Isolation/references/buffers/MCU add to bom count significantly
- isolated amplifiers are unwieldy, can't handle the common mode by themselves, and are expensive.
Thanks for all of your input!