This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA331: INA331 Output Voltage swing with gain < 10

Part Number: INA331
Other Parts Discussed in Thread: INA231, INA326

I'm using the INA331 with a gain of 5 and Vs = 5V. I'm getting a maximum Vout of 4.3V. Data sheet states Vout will not go to rail with gains < 10 (only when gain set to 5). However, it doesn't provide information as to how close it will get and what this depends on- the output load? What can I expect for max. Vout from part-part? Is there another part that doesn't have this shortcoming? The INA231 has the same thing.

  • Hello Dan,

    We have measured the linear operating region for the INA331 at a gain of 5V/V and at a higher gain (26.6V/V to be exact). The measured data at a gain of 5V/V corresponds well with the plot given in the data sheet and shown below. Therefore I would use the plot below to determine your output swing for gains <10V/V.  When measured in a gain of 26.6V/V the output was in fact rail-to-rail.  These limits depend more on internal amplifier common-mode input and output swing limitations than on output load.


    If you are looking for a single-supply RRI/O instrumentation amplifier even for gains <10V/V, I recommend evaluating the INA326.

    I hope this helps!

  • Thanks for the graph and info Pete. Yes I saw this, and based on the graph our output will only get to 4V (+/-?) with any + input greater than about 0.9V. We are lucky to be getting the 4.3V and not just 4V. So, you don't have a Vout min with Vin > 0.9V? Based on the graph I will have to use 3.9V to have some margin. There is only 1V horizontal scale.
    Thanks
    Dan
  • Hello Dan,

    It sounds like your understanding is correct, but keep in mind that it's for gains <10V/V. The Voutmin is listed in the typical specifications table as "Output voltage swing from Rail". For a load of 10kohms, the minimum specification is 50mV while the typical is 25mV. Of course this assumes that the device is operated according to the conditions listed at the top of the datasheet.
  • I still need the tolerance on the 4V output when I'm using a gain of 5. Sound like this data is not available.