I am currently working on an automatic sun tracking system consisting of a 85 W solar panel, microcontroller, and stepper motor. I need to monitor the output power of the solar panel at regular intervals. I was wondering if the INA209 chip would satisfy my requirements, and if it did, how should I  connect it to the panel, in order to monitor the output power?