I'm looking for a voltage input log amp for use as a wide dynamic range current sense amplifier. If this device has an input range of 100pA to 10mA, whats preventing me from using a resistor at the input sized to produce that current range (assuming I1 input is 0V)?
Specifically, I have a current that will generally be quite low, however can peak up to 400A, going through a 0.5mOhm sense resistor. This will create a 200mV worst case, which across 20Ohm will create 10mA. If this amp works down to 100pA, then i should be able to sense down to 4uA in this configuration. When I simulate this IC, I don't get results coming close to this. Page 18 of the datasheet says voltage input is limited, but doesn't give much of an explanation why.